what's different between MCIMX536AVV8C and MCIMX535DVV1C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what's different between MCIMX536AVV8C and MCIMX535DVV1C

1,581 次查看
Danial
Contributor II

Hello, every one!  I want to know what's different between MCIMX536AVV8C and MCIMX535DVV1C, who

can help me?  Or is there some datasheet about this? Thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,421 次查看
hippo
NXP TechSupport
NXP TechSupport

MCIMX536AVV8C is targeted for Automotive and Infotainment, while MCIMX535DVV1C is targeted for Consumer.

Their packages are same <http://www.freescale.com/files/shared/doc/package_info/98ASA00167D.pdf>, and they are pin to pin compatible.

You may refer to the Order Information in the datasheets or click i icon after buy one chip directly from www.freescale.com to learn more information about every part number.

1,421 次查看
Yuri
NXP Employee
NXP Employee

From the datasheet (for i.MX53xA, Automotive and Infotainment Applications Processors,
IMX53AEC, Rev. 4, 11/2011) :

MCIMX536AVV8C, mask N78C, 800 MHz, full feature set, 19 x 19 mm, 0.8 mm pitch BGA, Case TEPBGA-2


 

From the datasheet  (for i.MX53xD Applications Processors for Consumer Products,
IMX53CEC, Rev. 4.1, 2/2012) :

  MCIMX535DVV1C, mask N78C, 1 GHz, full feature set, temperature -20 to +85, 19 x 19 mm, 0.8 mm pitch BGA, Case TEPBGA-2