hI,
I need to know the name of this capacitors (on the L5 inductor side). My question (as schematic of the PMIC in the link below) is that in the U4B pmic figure there are 4.7U/10V/X5R-C2 and 0.1U/16V/X5R-C1 on the left side and 22U/6.3V/ X5R-C2 on the right side . Which one are the photo capacitors?
LINK:
pico-imx7d SOM board is not designed by NXP, but Technexion. The board we released is MCIMX7D-SabreSDB, so if you want to know more information about these capacitors, you will have to check it's design files of PCB Layout.
We don't have the design files of pico-imx7d SOM, so I have no way to help you check it.
The bettery way for you is to contact Technexion FAE or engineers.
Have a nice day!
BR,
Weidong