HDMI phy pll not locked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI phy pll not locked

1,079 Views
endl
Contributor II

Hello

I'm using "iMX 6Series Plarform SDK v1.1.0" for my i.MX6 DualLite processor.

I'm trying to use HDMI for image rendering but when I run the hdmi_test() from hdmi driver, I get the message: "PHY PLL not locked" and the test failed.

HDMI_IH_PHY_STAT0.TX_PHY_LOCK status bit is clear, but HDMI_PHY_STAT0.TX_PHY_LOCK status bit is set. What is the difference between these status registers ?

Why is PLL not locked ?

Thanks in advance.

Labels (2)
0 Kudos
Reply
1 Reply

867 Views
Yuri
NXP Employee
NXP Employee

  Please check if the HDMI test working on Freescale board (SDB / SDP).

Is I2C on Your board the same as for the SDP?

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply