Dear NXP,
I am working on Android 9 Automotive with IMX8QM. I am using LVDS to HDMI converter to connect between BOARD and Display.
ls /sys/class/drm/
card0 card1 version
Thanks & Regards,
VinothS,
Solved! Go to Solution.
Hi,
HDMI is working properly after flash
"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".
Regards,
VinothS,
Hi,
HDMI is working properly after flash
"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".
Regards,
VinothS,
Hi VinothS,
I’m afraid that the i.MX8QM is still on preproduction, and you need to contact with your Sales or FAE in case of requiring support.
Additionally, Android Auto is supported under “Commercial Support and Engineering Services” scheme. You could refer to the following link for additional details:
Commercial Support and Engineering Services | NXP
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Thank you CarlosCasillas,
Regards,
VinothS,