Hi,
I am working on HDMI - HDMI firmware is loading is proper with single bootloader, but dual bootloader firmware loading is not proper,
Single bootloader:
u-boot-imx8qm.imx
=> md 0x84002000
84002000: 00000506 22222211 e0000000 30000054 ....."""....T..0
84002010: 00000000 00000000 e400000c 00612013 ............. a.
84002020: 51fff921 f961fff9 7d030cff 10665002 !..Q..a....}.Pf.
84002030: 00000806 00000000 00000000 00000000 ................
84002040: 00506340 f03d0020 500020f0 b3b6c033 @cP. .=.. .P3...
84002050: 41747014 67344070 6340e513 c0335050 .ptAp@4g..@cPP3.
84002060: 00edb3f6 e8510020 7d030cff 34407002 .... .Q....}.p@4
84002070: 5050e340 7470c033 f0b3f641 12002030 @.PP3.ptA...0 ..
84002080: 491001a0 13480013 02002010 ad4500a0 ...I..H.. ....E.
84002090: 00000000 00000000 00000000 00000000 ................
840020a0: 00000000 00000000 00000000 00000000 ................
840020b0: 00000000 00000000 00000000 00000000 ................
840020c0: 00000000 00000000 00000000 00000000 ................
840020d0: 00000000 00000000 00000000 00000000 ................
840020e0: 00000000 00000000 00000000 00000000 ................
840020f0: 00000000 00000000 00000000 00000000 ................
Dual bootloader:
spl-imx8qm.bin & bootloader-imx8qm.img - Android Automotive Trusty bootloader
=> md 0x84002000
84002000: fffe6570 ffff0000 7fff0000 ffff177f pe..............
84002010: ffef0000 fffc0001 ffee0001 ffffc530 ............0...
84002020: ffef0000 ffff725e ffff0020 ffef7276 ....^r.. ...vr..
84002030: ffef0000 ffff0000 ffef0000 ffff9b8f ................
84002040: ffff0020 fffe0003 7ffe0001 ffffcc3c ...........<...
84002050: ffff0000 ff7f7256 ffff0000 ffff7256 ....Vr......Vr..
84002060: ffff0000 ffff0000 ffef0010 ffff6498 .............d..
84002070: ffff0040 ffff0001 ffff0003 ffbfc3e0 @...............
84002080: ffff0000 ffff7276 7fee0000 ffef7276 ....vr......vr..
84002090: fffe0000 ffef0000 ffef0000 ffff9b1f ................
840020a0: ffff0000 fffe0003 ffff0007 ffffd1e8 ................
840020b0: ffff0040 ffff7256 ffff0000 ffef7266 @...Vr......fr..
840020c0: ffff0002 ffff0000 7fff0022 ffff78aa ........"....x..
840020d0: fffe0000 ffef0023 ffff0006 fffec8a4 ....#...........
840020e0: ffef0002 ffff725e ffef0000 ffff72d6 ....^r.......r..
840020f0: ffee0040 ffff0000 ffff0004 fffe65bf @............e..
Is there any problem with dual bootloader ?
Is there any problem with trusty OS ?
Solved! Go to Solution.
Hi @igorpadykov ,
Finally, the issues are resolved long time back. For Android Automotive build, the hdmitx firmware was removed from final image.
Hi Vinothkumar
for narrowing down issue may be recommended to check it in latest nxp linux and android releases
Best regards
igor
Hi @igorpadykov ,
Finally, the issues are resolved long time back. For Android Automotive build, the hdmitx firmware was removed from final image.
Thank you Igor for the reply.
I fix this issue now.
I unable to update the patch and also I unable to add my HDMI TX changes in NXP knowledge base
If you are guide me, I will share and it will help to NXP Community.
one can try to get help through Live Chat [in section SUPPORT]
Best regards
igor