Hello Team,
My customer is a plan to use imx8m mini EVK and imx8mplus EVK in their project and they want to add support for operating with Larid 60-2230C wifi module based on M. 2 socket (PCIe+USB)
https://www.lairdconnect.com/wireless-modules/wifi-modules-bluetooth/60-2230c-series-bluetooth-and-w...
as I understand the IMX8M Plus EVK is configured by default to use M. 2 Module so adding such wifi module as above should be out of box experience, please correct me if I am wrong?
secondly, regards the imx8m MINI EVK, in order to prepare the kit to support M.2 I should do the following process
in order to load the NXP/Marvel wifi driver (which comes on every NXP/Freescale BSP), I make a new conf file such as wifi_mod_para_8997.conf file which contain the below:
PCIE8997 = {
cfg80211_wext=0xf
wfd_name=p2p
max_vir_bss=1
cal_data_cfg=none
drv_mode=7
ps_mode=2
auto_ds=2
fw_name=nxp/pcieuart8997_combo_v4.bin
}
and for loading into the kernel using the following command
“modprobe moal mod_para=nxp/wifi_mod_para_8997.conf”
Please advise back if I missed anything?
Waiting for your kind feedback, Thanks.
Regards,
Shai
Hello @shai_b ,
your configuation file is no problem.
pcieuart8997_combo_v4.bin should be copied to /lib/firmware/nxp
In additon, by default, for i.mx8mp-evk, 88w8997 has been supported in linux bsp.
Have a good day!
Regards,
weidong
Hello @weidong_sun,
Thank you so much for your support, I just got our imx8-mini evk with 88W8997 2x2 wifi module that works great via M.2 port.
I also updated my AP configuration that will work on WiFi5 on 5Ghz ("/etc/hostapd.conf"), I am sharing that for whom is relevant
interface=uap0
hw_mode=a
channel=0
country_code=US
ssid=NXP_Demo
auth_algs=1
ieee80211n=1
ieee80211ac=1
wpa=2
wpa_key_mgmt=WPA-PSK
rsn_pairwise=CCMP
wpa_passphrase=123456789
I have managed to set up the WLAN interface as AP and STA, but now I getting struggling to make the repeater mode (which is making a virtual WLAN instead of using LAN)
Can you please advise how to set up an AP that the internet source is from WLAN as well (WLAN0 <-> WLAN1)?
Waiting for your kind feedback, Thanks a lot.
KR,
Shai
Hi @weidong_sun,
I've opened a new thread here:
Have the internet connection using a station(WLAN0) and then bridge it to the AP interface(uap0)
Waiting for your feedback, Many Thanks.
KR,
Shai
Hello Team,
There is any feedback, Thanks in advance
KR,
Shai