Hi
I am using kernel 3.10.53
How can temperature be determined here
since i can see below entries in
/sys/devices/virtual/thermal
cooling_device0
cooling_device1
thermal_zone0
thermal_zone1
Regards
Himanshu
Hi ,
I recently did a short study on the temperature related stuffs and I saw when my yocto BSP is booting in i.MX6 Solo it shows the temperature as 41 degree Celsius and the print comes from the U-boot code which handles the temperature sensor part So I believe it is the temperature sensor value which is nothing but the on-die temperature
Then I checked the /sys/class/thermal/thermalzone1/temp value which is 43 degree Celsius . According to your answer, the sysfs shows CPU temperature. I can across various kind of temperature such as case temperature, junction temperature, die-temperature when the actual CPU temperature is considered. Can you be specific which temperature /sys/class/thermal/thermalzone1/temp actually points to .
Thanks & Regards,
Anjali