Get the temperature of i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get the temperature of i.mx6

Jump to solution
22,714 Views
carmilili
Contributor III

Hello,

     How can I get the temperature of the kernel of i.mx6q? The linux code is LTIB.

     Thank you.

Labels (3)
1 Solution
9,681 Views
justin_jiang
NXP Employee
NXP Employee

you can use "cat /sys/class/thermal/thermal_zone0/temp" to get the CPU temperature.

View solution in original post

10 Replies
9,681 Views
justin_jiang
NXP Employee
NXP Employee

The internal thermal sensor need calibration data which is burned in fuse to get an accurate temperature..

0 Kudos
Reply
9,681 Views
justin_jiang
NXP Employee
NXP Employee

This is not real degrees for temp. All the chip will get calibrations and you can use this data to get real temp with calibration data.

0 Kudos
Reply
9,681 Views
jonathanjuges
Contributor I

Hi,

Whenever I run: 

"cat /sys/class/thermal/thermal_zone0/temp"

I get:

42932

or similar numbers (42334).

Can anybody tell me what's going on? Thanks! 

0 Kudos
Reply
9,681 Views
himanshugusain
Contributor III

Hi

I am using kernel 3.10.53

How can temperature be determined here

since i can see below entries in

/sys/devices/virtual/thermal

cooling_device0

cooling_device1

thermal_zone0

thermal_zone1

Regards

Himanshu

0 Kudos
Reply
9,681 Views
justin_jiang
NXP Employee
NXP Employee

check the entry of thermal_zone0

9,682 Views
justin_jiang
NXP Employee
NXP Employee

you can use "cat /sys/class/thermal/thermal_zone0/temp" to get the CPU temperature.

9,681 Views
anjalikkrishna
Contributor III

Hi ,

 I recently did a short study on the temperature related stuffs and I saw when my yocto BSP is booting in i.MX6 Solo it shows the temperature as 41 degree Celsius and the print comes from the U-boot code which handles the temperature sensor part  So I believe it is the temperature sensor value which is nothing but the on-die temperature

Then I checked the /sys/class/thermal/thermalzone1/temp  value which is 43 degree Celsius . According to your answer, the sysfs shows CPU temperature. I can across various kind of temperature such as case temperature, junction temperature, die-temperature  when the actual CPU temperature is considered. Can you be specific  which temperature /sys/class/thermal/thermalzone1/temp actually points to .

Thanks & Regards,

Anjali

0 Kudos
Reply
9,681 Views
SantiagoVillafu
Contributor II

Hello, is that temperature given in Celsius degrees or Fahrenheit degrees? Thanks!

cat /sys/class/thermal/thermal_zone0/temp

53

0 Kudos
Reply
9,681 Views
justin_jiang
NXP Employee
NXP Employee

Celsius degrees

9,681 Views
carmilili
Contributor III

Thank you for your help.

0 Kudos
Reply