I am working on pwm audio driver, i got some pwm driver from below link:
GitHub - Glowforge/kernel-module-imx-pwm-audio: i.MX6 PWM audio driver
Please look at this driver once from above..............................
code from driver... "sdma-params" passing from device tree |
---|
/* Read SDMA channel number and load address */ if (of_property_read_u32_array(pdev->dev.of_node, "sdma-params", sdma_params, ARRAY_SIZE(sdma_params)) == 0) { // if (of_property_read_u32_array(pdev->dev.of_node, NULL, // NULL,0)) { self->sdma_ch_num = sdma_params[0]; self->sdma_script_origin = sdma_params[1]; } else { dev_err(&pdev->dev, "sdma-params property not specified"); goto failed_sdma_init; } |
while passing the parameters of sdma(channel No. and address of sdma script load address ) in devicetree the board is not booting(its booting till bootloader), is because of channel number and address?
Devicetree |
---|
&pwm3 { comaptible = "glowforge,imx-pwm-audio"; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_pwm3>; enable-gpio = <&gpio1 4 0>; timer = <0x10>; sdma-params = <0x19 0xdc0>; status = "okay"; |
Please suggest me how to pass these parameters through devicetree and also give some examples to understand it.
Thanks & Regards
Ganesh K
maybe you can check the Medium Quality Sound (MQS) of i.MX6UL to see if meet your requirements.