i.MX6 soloX MMC and eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 soloX MMC and eMMC

Jump to solution
1,948 Views
kmh48301
Contributor IV

Hi.

I have been studying about i.MX6 SoloX Boot with IMX6SXRM.

And In this Document, eMMC and MMC are confusing me...

 

The example below

kmh48301_3-1614294029558.png

 

 

MMC vs eMMC what's difference? when it comes to in this document.

=====================================================================

Question about : https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf

 

kmh48301_4-1614294029652.png

 

Due to my poor english, I don't understand the red box...

 

<my sabresd board>

kmh48301_5-1614294030102.png

 

 

Does the red box mean remove this sd card and connect to eMMC???

 

 

Please help me

 

Thanks

Best regards

Phillip

0 Kudos
1 Solution
1,911 Views
joanxie
NXP TechSupport
NXP TechSupport

current imx6 solox  sabresd board doesn't include emmc, pls refer to the schematic:

joanxie_0-1614745019875.png

if you want to use it, you can solid on this footprint

 

View solution in original post

0 Kudos
5 Replies
1,933 Views
joanxie
NXP TechSupport
NXP TechSupport

your picture is too small to read, do you mind telling where you get the information? the document and chapter name, thanks

 

0 Kudos
1,926 Views
kmh48301
Contributor IV

Hi

 

Sorry, I didn't know that.

 

First picture is in i.mx6 soloX Reference Manual Page 385 (Chapter 8.5.3.1)

 

Second picture is in i.MX Linux Release Notes Rev.L5.4.70_2.3.0-31 December 2020 Page 26~32

( I extracted the one that is related to mmc and emmc)

 

 

My question is still same.

MMC vs eMMC is confusing in documents.

and what does the red box mean in second picture?

 

0 Kudos
1,912 Views
joanxie
NXP TechSupport
NXP TechSupport

current imx6 solox  sabresd board doesn't include emmc, pls refer to the schematic:

joanxie_0-1614745019875.png

if you want to use it, you can solid on this footprint

 

0 Kudos
1,770 Views
vinythambi
Contributor I

Hi,

Do you have AVL(alternate vendor list) for the emmc? or can i use any emmc part?

The part in the reference design MTFC8GLCDM is obsolete.

0 Kudos
1,755 Views
joanxie
NXP TechSupport
NXP TechSupport
Hynix eMMC        
Cell Type Density PN eMMC Package Process
MLC 8GB H26M42003GMR V4.5 11.5 x 13 x 1.0 20nm
MLC 16GB H26M54003EMR V4.5 11.5 x 13 x 1.0 20nm
MLC 16GB H26M52003EQR V4.5 12 x 16 x 1.0 20nm
MLC 32GB H26M64003DQR V4.5 12 x 16 x 1.0 20nm
Micron eMMC      
Cell Type Density PN eMMC Package Process
MLC 16GB MTFC16GJUEF-AIT V4.41 14.0 x 18.0 x 1.2 25nm
MLC 32GB MTFC32GJUEF-AIT V4.41 14.0 x 18.0 x 1.2 25nm
MLC 16GB MTFC16GJVEC-4M IT V4.41 14.0 x 18.0 x 0.8 25nm
MLC 32GB MTFC32GJVED-4M IT V4.41 14.0 x 18.0 x 1.0 25nm
Samsung eMMC      
Cell Type Density PN eMMC Package Process
MLC 16GB KLMAG2GEAC-B001 V4.5 11.5 x 13 x 1.0 1xnm
MLC 32GB KLMBG4GEAC-B001 V4.5 11.5 x 13 x 1.0 1xnm
TLC 8GB KLM8G1WE4A-A001 V4.41 12 x 16 x 1.0 21nm
TLC 16GB KLMAG2WE4A-A001 V4.41 12 x 16 x 1.0 21nm
TLC 32GB KLMBG4WE4A-A001 V4.41 12 x 16 x 1.0 21nm
           
Toshiba eMMC V4.41 - 24nm; V4.41α & V4.5 - 19nm    
Cell Type Density PN eMMC Package Process
MLC 4GB THGBM4G5D1HBAIR 4.41 11.5 x 13 x 1.0 24nm
MLC 32GB THGBM4G8D4GBAIE 4.41 12 x 16 x 1.2 24nm
MLC 4GB THGBM5G5A1JBAIR V4.41α 11.5 x 13 x 1.0 19nm 
MLC 8GB THGBM5G6A2JBAIR V4.41α 11.5 x 13 x 1.0 19nm
MLC 16GB THGBM5G7A2JBAIR V4.41α 11.5 x 13 x 1.0 19nm
MLC 32GB THGBM5G8A4JBAIR V4.41α 11.5 x 13 x 1.0 19nm
           
Sandisk eMMC V4.5 - 19nm(only MLC)    
Cell Type Density PN eMMC Package Process
MLC 2GB SDIN5D2-2G 4.41 11.5 x 13 x 1.2 32nm
MLC 8GB SDIN5D2-8G 4.41 11.5 x 13 x 1.0 32nm
MLC 8GB SDIN5C2-8G 4.41 12 x 16 x 1.0 32nm
TLC 16GB SDIN5C1-16G 4.41 12 x 16 x 1.0 32nm