Hi Rambabu,
Please Check: GPS Testing on IMX6qsabresd board
Datasheet of Locosys AH-1613 GPS | NXP Communi
also, this should run on lastest bsp and python:
GitHub - Knio/pynmea2: Python library for parsing the NMEA 0183 protocol (GPS)
Hope this helps
hi;
Thanks for your Reply.
I am using VAR-SOM-MX6 android build for our custom imx6 board but in
VAR-SOM-MX6 android build there is no supported to AH-1613 gps module.
I am using ttymxc2 for gps. Here problem is that gps app not working and
I add my log messages also
root@var_som_mx6:/dev # ls -l
-rrr-- root root 131072 1970-01-01 00:00 __properties__
crw-rw-r-- system radio 10, 52 1970-01-01 00:00 alarm
crw-rw---- adb adb 10, 56 1970-01-01 00:00 android_adb
crw