Footnote 4 of eSDHC Input Hold Time (SD8) of i.MX6D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Footnote 4 of eSDHC Input Hold Time (SD8) of i.MX6D

ソリューションへジャンプ
846件の閲覧回数
takayuki_ishii
Contributor IV

Hello community.

 

I have one question about footnote4 of SD/MMC Interface Timing Specification.

Table 50. SD/eMMC4.3 Interface Timing Specification in datasheet IMX6DQAEC Rev. 6, 11/2018 

It have footnote 4 as following,

4. To satisfy hold timing, the delay difference between clock input and cmd/data input must not exceed 2 ns.

Is it meaning that each hold time between SD_CLK <-> SD_CMD, SD_CLK <-> SD_D1, SD_CLK <-> SD_D2 ... SD_CLK <-> SD_D7 must not exceed 2 ns ?

Please see attached document "SDR104_HoldTiming_2ns.xlsx".

 

Best regards,

Ishii.

 

 

0 件の賞賛
返信
1 解決策
834件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @takayuki_ishii,

 

Your understanding is correct, the time between data must not exceed 2nS.

 

Regards,

Israel.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
835件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @takayuki_ishii,

 

Your understanding is correct, the time between data must not exceed 2nS.

 

Regards,

Israel.

0 件の賞賛
返信