Flash i.MX6D via USB OTG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash i.MX6D via USB OTG

578 Views
paul_becue
Contributor I

What are the necessary settings and actions to do flash a "virgin" device (our own hardware with an i.MX6D on) using the USB OTG port of the i.MX6D?

Does the device act as an "USB stick" at that moment or is it slightly different?

How to start a device to this state when it is not virgin anymore?

Is there somewhere a checklist to see if nothing is forgotten?

Kind Regards.

Paul Becue.

Labels (4)
0 Kudos
Reply
1 Reply

472 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

nxp provides mfg tool application for such purposes, it acts as usb hid/msd device.

https://community.nxp.com/docs/DOC-332977 

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply