Hi team,
I am facing problem with fether failure when building image for imx6/imx53 boards.
linux-denx-3.9-r0 do_fetch: Failed to fetch URL git://git.denx.de/linux-denx.git;branch=, attempting MIRRORS if available
only this package isnt downloading , rest all the packages have been downloaded.
Any one have any other alternative for this ? how to setup local repo for this particular package?
Appreciate your help in this.
Thanks,
Dheeraj
已解决! 转到解答。
No martin,
I am not behind any Proxy or firewall.
here is the log:
WARNING: linux-denx-3.9-r0 do_fetch: Failed to fetch URL git://git.denx.de/linux-denx.git;branch=m28evk-2013-05-02-v3.9, attempting MIRRORS if available
ERROR: linux-denx-3.9-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/opt/poky/build/downloads/git2/git.denx.de.linux-denx.git'...
fatal: read error: Connection reset by peer
fatal: early EOF
fatal: index-pack failed
ERROR: linux-denx-3.9-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.denx.de/linux-denx.git;branch=m28evk-2013-05-02-v3.9'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /opt/poky/build/tmp/work/m53evk-poky-linux-gnueabi/linux-denx/3.9-r0/temp/log.do_fetch.88466
ERROR: Task 50 (/opt/poky/meta-fsl-arm-extra/recipes-kernel/linux/linux-denx_3.9.bb, do_fetch) failed with exit code '1'
Now , if i try to browse this package through Web, then also i ma unable to download it.
Is there an alternative way to do this? Any manual way ? I have been trying this since last one month and No luck. Upon googling i came across this post
https://lists.yoctoproject.org/pipermail/meta-freescale/2014-February/007111.html
Thanks,
Dheeraj