Fetcher Failure on Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fetcher Failure on Yocto

Jump to solution
10,042 Views
dheerajkumar
Contributor I

Hi team,


I am facing problem with fether failure when building image for imx6/imx53 boards.

linux-denx-3.9-r0 do_fetch: Failed to fetch URL git://git.denx.de/linux-denx.git;branch=, attempting MIRRORS if available

only this package isnt downloading , rest all the packages have been downloaded.

Any one have any other alternative for this ? how to setup local repo for this particular package?

Appreciate your help in this.

Thanks,

Dheeraj

Labels (3)
Tags (2)
0 Kudos
Reply
1 Solution
8,824 Views
martin_maurer
Contributor III

Are you behind a firewall (company network?) and perhaps using proxy for http/https?

View solution in original post

0 Kudos
Reply
2 Replies
8,825 Views
martin_maurer
Contributor III

Are you behind a firewall (company network?) and perhaps using proxy for http/https?

0 Kudos
Reply
8,824 Views
dheerajkumar
Contributor I

No martin,

I am not behind any Proxy or firewall.

here is the log:

WARNING: linux-denx-3.9-r0 do_fetch: Failed to fetch URL git://git.denx.de/linux-denx.git;branch=m28evk-2013-05-02-v3.9, attempting MIRRORS if available

ERROR: linux-denx-3.9-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/opt/poky/build/downloads/git2/git.denx.de.linux-denx.git'...

fatal: read error: Connection reset by peer

fatal: early EOF

fatal: index-pack failed

ERROR: linux-denx-3.9-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.denx.de/linux-denx.git;branch=m28evk-2013-05-02-v3.9'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /opt/poky/build/tmp/work/m53evk-poky-linux-gnueabi/linux-denx/3.9-r0/temp/log.do_fetch.88466

ERROR: Task 50 (/opt/poky/meta-fsl-arm-extra/recipes-kernel/linux/linux-denx_3.9.bb, do_fetch) failed with exit code '1'

Now , if i try to browse this package through Web, then also i ma unable to download it.

Is there an alternative way to do this? Any manual way ? I have been trying this since last one month and No luck. Upon googling i came across this post

https://lists.yoctoproject.org/pipermail/meta-freescale/2014-February/007111.html

Thanks,

Dheeraj

0 Kudos
Reply