Fastboot issue for IMX6DL Android Kitkat 4.4.3 KK4.4.3_2.0.0-ga

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fastboot issue for IMX6DL Android Kitkat 4.4.3 KK4.4.3_2.0.0-ga

1,244 次查看
zhanxiaozhang
Contributor III

when enter fastboot mode ,I type fastboot erase userdata command ,uart console shows "Not support erase command for EMMC".

Does uboot do not support emmc erase function, is there any patch for emmc fastboot erase?

Additional ,when use android Setting-->reset-factory----> , it reboot and  show "erasing " always ,can not achieve erasing ,the progress bar always animation,is there any bug with it ,and any patch for these?

标签 (1)
0 项奖励
回复
2 回复数

705 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Zhanxiao,

About "erase eMMC", you can refer to the link:

https://community.freescale.com/thread/377766

(It seems that u-boot doesn't support erase eMMC with partitions)

For recovery method, please refter to FAQ documents released with Android Kitkat 4.4.3 . In the section of 8.2 How do I use Android fastboot.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

705 次查看
zhanxiaozhang
Contributor III

I means erase partition. not mmc command.

0 项奖励
回复