Fastboot issue for IMX6DL Android Kitkat 4.4.3 KK4.4.3_2.0.0-ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fastboot issue for IMX6DL Android Kitkat 4.4.3 KK4.4.3_2.0.0-ga

1,337 Views
zhanxiaozhang
Contributor III

when enter fastboot mode ,I type fastboot erase userdata command ,uart console shows "Not support erase command for EMMC".

Does uboot do not support emmc erase function, is there any patch for emmc fastboot erase?

Additional ,when use android Setting-->reset-factory----> , it reboot and  show "erasing " always ,can not achieve erasing ,the progress bar always animation,is there any bug with it ,and any patch for these?

Labels (1)
0 Kudos
Reply
2 Replies

798 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Zhanxiao,

About "erase eMMC", you can refer to the link:

https://community.freescale.com/thread/377766

(It seems that u-boot doesn't support erase eMMC with partitions)

For recovery method, please refter to FAQ documents released with Android Kitkat 4.4.3 . In the section of 8.2 How do I use Android fastboot.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

798 Views
zhanxiaozhang
Contributor III

I means erase partition. not mmc command.

0 Kudos
Reply