Hi all
Does someone have a information for external dimensions of MCIMX7SABRE ?
Ko-hey
解決済! 解決策の投稿を見る。
Hello Ko-hey,
the dimensions are ca 130x130 mm.
Best Regards,
Jan
Hi janspurek
Thank you for support.
Could you tell me the following things too ?
1.Position of 120 pin connector J13 (QSH - 060 - 01 - L - D - A)
2.Position and hole diameter of non-through hole at four corners
3.Substrate thickness
Ko-hey
Hello Ko-hey,
1. -151.771, 3746.522 [mills]
2. diameter: ca 127 mills
hole 1: -236.220, 4960.630 [mills]
hole 2: 4566.929, 4960.630 [mills]
hole 3: 4566.929, 157.480 [mills]
hole 4: -236.220, 157.480 [mills]
3. 56 mills (dielectrics only - each 8 mills), 65.6 mills (including the conductor layers - each 1.2 mills)
Please note that the coordinates apply to the centers of the objects.
Best Regards,
Jan