Hi all ,
We are working on our custom board based . its using imx6 and the ethernet is in RMII mode and phy is LAN8710A. Issues is once the kernel boots up we are getting continous log as shown below. We are able to use tftp from uboot promt . Also same images configurations we have tested on 10 boards. Only in 2 out of 10 we are facing this issue.
Below are our changes in uboot and kernel . Please verify the same. Is any initialization sequence missing ??
In u-boot-2009.08
board/freescale/customxxx/custom-boardxxx.c
int board_init(void) {
mxc_iomux_v3_init((void *)IOMUXC_BASE_ADDR);
setup_boot_device();
fsl_set_system_rev();
/* board id for linux */
gd->bd->bi_arch_number = 4412;
/* address of boot parameters */
gd->bd->bi_boot_params = PHYS_SDRAM_1 + 0x100;
setup_uart();
#ifdef CONFIG_NAND_GPMI
setup_gpmi_nand();
#endif
#if defined(CONFIG_ENET_RMII) && !defined(CONFIG_DWC_AHSATA)
setup_fec();
#endif
return 0;
}
static int setup_fec(void)
{
u32 reg = 0;
s32 timeout = 100000;
/*
* get enet tx reference clk from internal clock from anatop
* GPR1[21] = 1
*/
reg = readl(IOMUXC_BASE_ADDR + 0x4);
reg |= (0x1 << 21);
writel(reg, IOMUXC_BASE_ADDR + 0x4);
/* Enable PLLs */
reg = readl(ANATOP_BASE_ADDR + 0xe0); /* ENET PLL */
if ((reg & ANATOP_PLL_PWDN_MASK) || (!(reg & ANATOP_PLL_LOCK))) {
reg &= ~ANATOP_PLL_PWDN_MASK;
writel(reg, ANATOP_BASE_ADDR + 0xe0);
while (timeout--) {
if (readl(ANATOP_BASE_ADDR + 0xe0) & ANATOP_PLL_LOCK)
break;
}
if (timeout <= 0)
return -1;
}
/* Enable FEC clock */
reg |= ANATOP_FEC_PLL_ENABLE_MASK;
reg &= ~ANATOP_PLL_BYPASS_MASK;
writel(reg, ANATOP_BASE_ADDR + 0xe0);
return 0;
}
int board_eth_init(bd_t *bis)
{
int rc = -ENODEV;
return rc;
}
In include/asm-arm/arch-mx6/mx6dl_pins.h
#define MX6DL_PAD_RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT \
- IOMUX_PAD(0x06BC, 0x02D4, 7, 0x080C, 1, MX6DL_ENET_PAD_CTRL)
+ IOMUX_PAD(0x06BC, 0x02D4, 0x17, 0x080C, 1, MX6DL_ENET_PAD_CTRL)
Kernel Changes - linux-3.0.35
In "arch/arm/mach-mx6/board-ihmvisio7.c"
/*****************************************************************************
*
* Init FEC and AR8031 PHY
*
*****************************************************************************/
static int ihmvisio7_fec_phy_init(struct phy_device *phydev) { return 0; }
/* ------------------------------------------------------------------------ */
static int ihmvisio7_fec_power_hibernate(struct phy_device *phydev) { return 0; }
/* ------------------------------------------------------------------------ */
static struct fec_platform_data ihmvisio7_fec_data = {
.init = ihmvisio7_fec_phy_init,
.power_hibernate = ihmvisio7_fec_power_hibernate,
.phy = PHY_INTERFACE_MODE_RMII,
};
/* ------------------------------------------------------------------------ */
static __init void ihmvisio7_init_ethernet(void)
{
IMX6_SETUP_PAD(ENET_MDIO__ENET_MDIO); // SMI Data Input/ouput
IMX6_SETUP_PAD(ENET_MDC__ENET_MDC); // SMI clock
IMX6_SETUP_PAD(ENET_REF_CLK__ENET_TX_CLK); // reference clock
IMX6_SETUP_PAD(ENET_CRS_DV__ENET_RX_EN); //Carrier sense
IMX6_SETUP_PAD(ENET_RX_ER__ENET_RX_ER); // Receive error
IMX6_SETUP_PAD(ENET_TX_EN__ENET_TX_EN); // transmit enable
IMX6_SETUP_PAD(ENET_TXD0__ENET_TDATA_0); //RMII
IMX6_SETUP_PAD(ENET_TXD1__ENET_TDATA_1); //RMII
IMX6_SETUP_PAD(ENET_RXD0__ENET_RDATA_0); //RMII
IMX6_SETUP_PAD(ENET_RXD1__ENET_RDATA_1); //RMII
IMX6_SETUP_PAD(RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT); //RMII
IMX6_SETUP_PAD(SD4_DAT0__GPIO_2_8); // phy reset
gpio_request(ihmvisio7_RGMII_RST, "rgmii reset");
gpio_direction_output(ihmvisio7_RGMII_RST, 0);
#ifdef CONFIG_FEC_1588
mxc_iomux_set_gpr_register(1, 21, 1, 1);
#endif
msleep(10);
gpio_set_value(ihmvisio7_RGMII_RST, 1);
imx6_init_fec(ihmvisio7_fec_data);
}
Any initialization missing ?????
Error log on booting
PHY: 1:00 - Link is Up - 100/Full
PHY: 1:00 - Link is Down
PHY: 1:00 - Link is Up - 100/Full
PHY: 1:00 - Link is Down
PHY: 1:00 - Link is Up - 10/Full
filesystem built on Thu, 27 Feb 2014 11:04:53 +0530
xxx login: root
Password:
login[2612]: root login on 'ttymxc1'
root@xxx ~$
Regards
sn ng
Hi sn
if such behaviour is on some boards this may be just hardrware issue:
poor soldering or bad contact on board connector.
Best regards
igor
Hi igor ,
But we doubt if some phy (LAN8710A) initialization is missing in kernel as the board seems to attain ip after some up -down-up-down logs..
In kernel we have added these changes --
Kernel Changes - linux-3.0.35
In "arch/arm/mach-mx6/board-ihmvisio7.c"
/*****************************************************************************
*
* Init FEC and AR8031 PHY
*
*****************************************************************************/
static int ihmvisio7_fec_phy_init(struct phy_device *phydev) { return 0; }
/* ------------------------------------------------------------------------ */
static int ihmvisio7_fec_power_hibernate(struct phy_device *phydev) { return 0; }
/* ------------------------------------------------------------------------ */
static struct fec_platform_data ihmvisio7_fec_data = {
.init = ihmvisio7_fec_phy_init,
.power_hibernate = ihmvisio7_fec_power_hibernate,
.phy = PHY_INTERFACE_MODE_RMII,
};
/* ------------------------------------------------------------------------ */
static __init void ihmvisio7_init_ethernet(void)
{
IMX6_SETUP_PAD(ENET_MDIO__ENET_MDIO); // SMI Data Input/ouput
IMX6_SETUP_PAD(ENET_MDC__ENET_MDC); // SMI clock
IMX6_SETUP_PAD(ENET_REF_CLK__ENET_TX_CLK); // reference clock
IMX6_SETUP_PAD(ENET_CRS_DV__ENET_RX_EN); //Carrier sense
IMX6_SETUP_PAD(ENET_RX_ER__ENET_RX_ER); // Receive error
IMX6_SETUP_PAD(ENET_TX_EN__ENET_TX_EN); // transmit enable
IMX6_SETUP_PAD(ENET_TXD0__ENET_TDATA_0); //RMII
IMX6_SETUP_PAD(ENET_TXD1__ENET_TDATA_1); //RMII
IMX6_SETUP_PAD(ENET_RXD0__ENET_RDATA_0); //RMII
IMX6_SETUP_PAD(ENET_RXD1__ENET_RDATA_1); //RMII
IMX6_SETUP_PAD(RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT); //RMII
IMX6_SETUP_PAD(SD4_DAT0__GPIO_2_8); // phy reset
gpio_request(ihmvisio7_RGMII_RST, "rgmii reset");
gpio_direction_output(ihmvisio7_RGMII_RST, 0);
#ifdef CONFIG_FEC_1588
mxc_iomux_set_gpr_register(1, 21, 1, 1);
#endif
msleep(10);
gpio_set_value(ihmvisio7_RGMII_RST, 1);
imx6_init_fec(ihmvisio7_fec_data);
}
Can you please confirm our doubt ??
Regards
sn