ETH_VDDIO on SabreSD i.MX6 Quad EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ETH_VDDIO on SabreSD i.MX6 Quad EVK

662 次查看
vincentchou
Contributor IV

Dear support,

Based on the i.MX6 EVK schematic, ETH_VDDIO should be 1.8V or 2.5V.  Unfortunately we accidentally wired 3.3V to ETH_VDDIO to NVCC_RGMII on our board.  Luckily we don't use any Ethernet components on our board.  I would like to ask your opinion whether this voltage will cause problem of the operation of the board and the CPU?

Vincent

标签 (4)
0 项奖励
回复
1 回复

605 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

i.MX6Q max. NVCC_RGMII  is 2.625V according to Table 6. Operating Ranges

Table 6. Operating Ranges i.MX6DQ Datasheet, so 3.3V may cause problems to processor.

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复