Hi,
I use ESAI with the following specifications.
・TDM 14 slot transmit/receive
・Use Pin of ESAI_RX_CLK, ESAI_RX_FS, ESAI_RX_HF_CLK, ESAI_TX0, ESAI_TX5_RX0, ESAI_TX_CLK, ESAI_TX_FS,
ESAI_TX_HF_CLK.
Question.
1)I use only ESAI_TX0, and can you transmit 14 TDM slot?
Please tell me the method to transmit TDM 14slot if it is failure.
2)I use only ESAI_TX5_RX0, and can you receive 14 TDM slot?
Please tell me the method to receive TDM 14slot if it is failure.
Best regards,
soichi
解決済! 解決策の投稿を見る。
Hi Soichi
number of slots (words) is defined by TDC field ESAI_TCCR
register. Example for ESAI can be found in SDK ..drivers/audio,
pay attention to "channel_number" parameter. Description in
Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf
"MX6_PLATFORM_SDK "
https://community.freescale.com/docs/DOC-94139
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Soichi
number of slots (words) is defined by TDC field ESAI_TCCR
register. Example for ESAI can be found in SDK ..drivers/audio,
pay attention to "channel_number" parameter. Description in
Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf
"MX6_PLATFORM_SDK "
https://community.freescale.com/docs/DOC-94139
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI. I cannot download the document,
It says "Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."
you can try to request it from below link