ESAI of TDM slot for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ESAI of TDM slot for i.MX6

跳至解决方案
1,273 次查看
soichiyamamoto
Contributor V

Hi,

I use ESAI with the following specifications.

・TDM 14 slot transmit/receive

・Use Pin  of  ESAI_RX_CLK, ESAI_RX_FS, ESAI_RX_HF_CLK, ESAI_TX0, ESAI_TX5_RX0, ESAI_TX_CLK, ESAI_TX_FS,

ESAI_TX_HF_CLK.

Question.

1)I use only ESAI_TX0, and can you transmit 14 TDM slot?

 Please tell me the method to transmit TDM 14slot if it is failure.

2)I use only ESAI_TX5_RX0, and can you receive 14 TDM slot?

 Please tell me the method to receive TDM 14slot if it is failure.

Best regards,

soichi

标签 (1)
0 项奖励
回复
1 解答
801 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

number of slots (words) is defined by TDC field ESAI_TCCR

register. Example for ESAI can be found in SDK ..drivers/audio,

pay attention to "channel_number" parameter. Description in

Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf

"MX6_PLATFORM_SDK "

https://community.freescale.com/docs/DOC-94139

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
802 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

number of slots (words) is defined by TDC field ESAI_TCCR

register. Example for ESAI can be found in SDK ..drivers/audio,

pay attention to "channel_number" parameter. Description in

Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf

"MX6_PLATFORM_SDK "

https://community.freescale.com/docs/DOC-94139

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
801 次查看
charles_chang
Contributor I

HI.  I cannot download the document,

It says "Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."

0 项奖励
回复
801 次查看
igorpadykov
NXP Employee
NXP Employee

you can try to request it from below link

https://community.freescale.com/message/556724#556724

0 项奖励
回复