ESAI of TDM slot for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ESAI of TDM slot for i.MX6

Jump to solution
1,274 Views
soichiyamamoto
Contributor V

Hi,

I use ESAI with the following specifications.

・TDM 14 slot transmit/receive

・Use Pin  of  ESAI_RX_CLK, ESAI_RX_FS, ESAI_RX_HF_CLK, ESAI_TX0, ESAI_TX5_RX0, ESAI_TX_CLK, ESAI_TX_FS,

ESAI_TX_HF_CLK.

Question.

1)I use only ESAI_TX0, and can you transmit 14 TDM slot?

 Please tell me the method to transmit TDM 14slot if it is failure.

2)I use only ESAI_TX5_RX0, and can you receive 14 TDM slot?

 Please tell me the method to receive TDM 14slot if it is failure.

Best regards,

soichi

Labels (1)
0 Kudos
Reply
1 Solution
802 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

number of slots (words) is defined by TDC field ESAI_TCCR

register. Example for ESAI can be found in SDK ..drivers/audio,

pay attention to "channel_number" parameter. Description in

Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf

"MX6_PLATFORM_SDK "

https://community.freescale.com/docs/DOC-94139

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
803 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

number of slots (words) is defined by TDC field ESAI_TCCR

register. Example for ESAI can be found in SDK ..drivers/audio,

pay attention to "channel_number" parameter. Description in

Chapter 9 Configuring the ESAI Driver iMX6_Firmware_Guide.pdf

"MX6_PLATFORM_SDK "

https://community.freescale.com/docs/DOC-94139

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
802 Views
charles_chang
Contributor I

HI.  I cannot download the document,

It says "Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."

0 Kudos
Reply
802 Views
igorpadykov
NXP Employee
NXP Employee

you can try to request it from below link

https://community.freescale.com/message/556724#556724

0 Kudos
Reply