ERROR : I.MX8MQ EVK yocto compilation in opencv

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR : I.MX8MQ EVK yocto compilation in opencv

ソリューションへジャンプ
2,752件の閲覧回数
dhaval_shah
Contributor II

Hi,

I am compiling the Rocko version of the yocto downloaded by using the following commands on the Ubuntu 16.04

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
repo sync

I have already installed all the required packages as per the yocto userguide.

And set the environment using the following commands.

DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build

and build using the following command.

DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk bitbake fsl-image-validation-imx

But, I am facing the compilation issue as follows in the opencv.

ERROR: opencv-3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0 do_fetch: Fetcher failure: Fetch command export PATH="/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/usr/bin/python3-native:/home/ankitrpatel/Project/rocko/sources/poky/scripts:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot/usr/bin/crossscripts:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/usr/sbin:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/usr/bin:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/sbin:/home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/recipe-sysroot-native/bin:/home/ankitrpatel/Project/rocko/sources/poky/bitbake/bin:/home/ankitrpatel/Project/rocko/build/tmp/hosttools"; export HOME="/home/ankitrpatel"; git -c core.fsyncobjectfiles=0 remote add --mirror=fetch origin git://github.com/opencv/opencv.git failed with exit code 128, output:
fatal: Not a git repository (or any of the parent directories): .git

ERROR: opencv-3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0 do_fetch: Fetcher failure for URL: 'git://github.com/opencv/opencv.git;name=opencv'. Unable to fetch URL from any source.
ERROR: opencv-3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/ankitrpatel/Project/rocko/build/tmp/work/aarch64-mx8mq-poky-linux/opencv/3.4+gitAUTOINC+6d4f66472e_81ca8dab86_a62e20676a_34e4206aef_fccf7cd6a4-r0/temp/log.do_fetch.22056

Can you please help me if someone has face same kind of issue.

I have already tried to set the export GIT_DISCOVERY_ACROSS_FILESYSTEM="1" and then tried but same issue is coming.

Thanks & Regards,

Dhaval

タグ(2)
0 件の賞賛
返信
1 解決策
2,216件の閲覧回数
dhaval_shah
Contributor II

Hi,

No need to put efforts, I have debug the issue with -D and get the solution for this issue.

This is because of some limitation in the local network because of larger file size download. Handle the issue by updating in local network rules.

Thanks & Regards,

Dhaval

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,216件の閲覧回数
molin_du
Contributor II

Hello Dhaval:

Thank you for your investigation.

In my case, the download "reach 100%" many times and "start again".

I saw you post so I just keep waiting, finally it really complete.

0 件の賞賛
返信
2,216件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Dhaval,

Thank you for posting your findings! I’m sure it will help other community users.

Regards,

0 件の賞賛
返信
2,217件の閲覧回数
dhaval_shah
Contributor II

Hi,

No need to put efforts, I have debug the issue with -D and get the solution for this issue.

This is because of some limitation in the local network because of larger file size download. Handle the issue by updating in local network rules.

Thanks & Regards,

Dhaval

0 件の賞賛
返信