We are trying to implement dual camera(both are ov5640) in imx8 m mini, but the processor has only one csi controller, is it possible to realize this?
Hallo,
is there any follow up on this topic?
I am facing the same issue. My application is for wearable device with dual camera. Regarding price and power consumption, iMx8 M mini is the better choice, I think.
But Mini has only one CSI lane. do we have any multiplexer boards available, so we can chose one camera at a time by GPIO ?
regards
Jane
Hello Anusha,
You can try one USB Camera and one MIPI CSI it should works.
Regards
Hi Sir,
imx8 m mini has only one csi controller, but we want to have two cameras(both ov5640) one as front camera and one as back camera.
My doubt is whether we can use two cameras on different i2c buses with one csi controller, we have a gpio to select the camera one at a time by making it high and low.
Hi Sir,
I have already gone through the link, but imx8 m mini has only one csi controller where as the soc mentioned in the link has two csi controllers from the processor.
My doubt is whether we can use two cameras on different i2c buses with one csi controller, we have a gpio to select the camera one at a time by making it high and low.