Psplash screen rotation on Yocto i.MX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Psplash screen rotation on Yocto i.MX7

927 Views
econote_vikrant
Contributor III

Greetings!

I'm working on a custom board with L5.10.72 Kernel BSP, in which the yocto boot logo is coming upside down (showing open-embedded as LOGO) through psplash.

We need to rotate that yocto boot logo to 90 degrees.

I would like to request the preliminary patch for the same.

 

Regards,
Vikrant

Labels (3)
0 Kudos
Reply
1 Reply

915 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @econote_vikrant 

You can rotate the origin image using image tool.

 

0 Kudos
Reply