Does the SRS (Software Reset Signal) Bit of the WDOG Register reset the system?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the SRS (Software Reset Signal) Bit of the WDOG Register reset the system?

Jump to solution
578 Views
simon_ko
Contributor III

I'm reviewing WDOG on the i.MX 8M Plus.

Page 973 of IMX8MPRM Rev.1 says that WDOG generates reset signal by SRS.

2023-01-09 00 59 41.png

 

However, the SRS bit description of WCR Register says that Software Reset is not generate in Block.

 

2023-01-09 01 01 36.png

 

I don't understand this part.
Please explain.

 

Thanks.

0 Kudos
Reply
1 Solution
557 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @simon_ko ,

I hope you are doing well.
 
It suggests that the SRS bit doesn't not necessarily resets the system as WDOG_RESET_B_DEB doesn't generate software reset directly. unlike wdog_b which can be used to reset PMIC.
 
WDOG_RESET_B_DEB is given as input to SRC(refer to Figure 6-31. SRC inputs and outputs in RM)  and the Reset functionality of cores can be configured using the SRC register.
 
One can refer to MASK_WDOG1_RST in 6.5.5.2 A53 Reset Control Register and  6.5.5.4 M7 Reset Control Register in RM for more information,
 
Thanks & Regards,
Sanket Parekh

View solution in original post

1 Reply
558 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @simon_ko ,

I hope you are doing well.
 
It suggests that the SRS bit doesn't not necessarily resets the system as WDOG_RESET_B_DEB doesn't generate software reset directly. unlike wdog_b which can be used to reset PMIC.
 
WDOG_RESET_B_DEB is given as input to SRC(refer to Figure 6-31. SRC inputs and outputs in RM)  and the Reset functionality of cores can be configured using the SRC register.
 
One can refer to MASK_WDOG1_RST in 6.5.5.2 A53 Reset Control Register and  6.5.5.4 M7 Reset Control Register in RM for more information,
 
Thanks & Regards,
Sanket Parekh