Does imx-yocto-L5.4.70_2.3.0 support rtsp streaming with rtsp-server in imx8qxp ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does imx-yocto-L5.4.70_2.3.0 support rtsp streaming with rtsp-server in imx8qxp ??

856 次查看
yibhan
Contributor III

Dear NXP,

I have questions for supporting rtsp streaming of camera.

I am using imx-yocto-L5.4.70_2.3.0 and image build is imx-image-full.

And I have checked libgstrtspserver-1.0.so.0 and libgstrtspserver-1.0.so.0.1602.0 in rootfs and sdk.

According to Doc. i.MX8 GStreamer User Guide, they recommands using "gst-variable-rtsp-server" when RTSP Streaming .

Is it possible to use gst-rtsp-server instead of gst-variable-rtsp-server?

My question is "Should I still add "gst-variable-rtsp-server" package for rtsp streaming in imx8qxp in yocto build?"

If you have any knowledge of rtsp streaming about imx8qxp, please give me any advices.

Thanks,

0 项奖励
回复
1 回复

854 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yibeom

 

one can try to follow sect.7.3.13 Real Time Streaming Protocol (RTSP) Linux Guide

included in L5.4.70_2.3.0 linux documentation package   Documentation

Also may be useful :

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-RTSP-Streaming-Support/ta-p/11217...

 

Best regards
igor

0 项奖励
回复