Does i.MX8MQ GIC have legacy modes?What is the address of GIC CPU interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX8MQ GIC have legacy modes?What is the address of GIC CPU interface?

3,180件の閲覧回数
pengcheng
Contributor III

What is i.MX8MQ GIC versoin number? GIC500?

Does i.MX8MQ GIC have legacy modes?

What is the memory address of GIC CPU interface?

Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
10 返答(返信)

2,641件の閲覧回数
pengcheng
Contributor III

Anyone can help me? Thanks!

0 件の賞賛
返信

2,641件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

According to the ARM processor documentation CBAR_EL1 register "holds the physical
base address of the memory-mapped GIC CPU interface registers”.

ARM Information Center 

Regards,

Yuri.

0 件の賞賛
返信

2,641件の閲覧回数
pengcheng
Contributor III

I can detect imx8mq has GIC-500 according to IIDR and PIDR register.

And did not support memory mapped CPU interface by testing other registers.

0 件の賞賛
返信

2,641件の閲覧回数
pengcheng
Contributor III

Recently I found that, software working in EL3 can change the SRE and ARE bit.

So if I want to use legacy mode for non-SRE, I must know the memory address of CPU-interface.

GICv3 is designed by ARM, that is right, but  it is connect to NOC by NXP.

NXP should know the memory address of CPU-interface.

My question is I want to know the memory address of CPU-interface to use the legacy mode.

So I reopen this issue.

Thanks!

0 件の賞賛
返信

2,641件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peng

please refer to sect.4.1.4 Platform sub-blocks i.MX8MDQ Reference Manual

and arm documentation

ARM Information Center 

https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

core revision is r0p4-51rel0, as described in sect.4.1.2 Configuration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,641件の閲覧回数
pengcheng
Contributor III

Hi igor,

Thanks!

But you don't answer my questions. I knew the GIC is GIC v4.

But I do not want to use <system registers enable> method, instead I want to use the legacy mode which will operates CPU interface by using memory-mapped regions.

So, my main question is:

1. Does i.MX8MQ GIC have legacy modes?

2. What is the memory-mapped address of GIC CPU interface?

BR,

Peng

0 件の賞賛
返信

2,641件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peng

GIC is module designed by arm, suggest to post it on arm forum.

Arm Development Platforms forum - Arm Development Platforms - Arm Community 

Best regards
igor

0 件の賞賛
返信

2,641件の閲覧回数
pengcheng
Contributor III

Hi igor,

Thanks!

I know GIC is designed by arm, but some parts are implemented by vendors. That is why I want to know which type is this GIC? GIC500?GIC600?

For example:

“Whether a GICv3 implementation includes a mechanism to support legacy operation of physical interrupts is
IMPLEMENTATION DEFINED.”

And also I think memory map is also implemented by vendors, ARM only support the register offset which are based on that memory block. 

Am I right?

BR,

Peng

0 件の賞賛
返信

2,641件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

GIC400 and its address is given in sect.2.1.2 Cortex-A53 Memory Map i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

Best regards
igor

0 件の賞賛
返信

2,641件の閲覧回数
pengcheng
Contributor III

Hi igor,

Thanks!

1. I don't think GIC400 is correct.

In page 565 of IMX8MDQLQRM. It said:

"The Cortex-A53 processor implements the GIC CPU interface as described in the
Generic Interrupt Controller (GICv4) architecture."

I think GIC400 is not GICv4 based. 

2. Also the memory map only refer that the GIC block.

"3880_0000 388F_FFFF GIC 1MB GIC REG"

But doesn't mention the address of CPU interface. And I can't find it in the linux code ether. I know it can be accessed by system register, but I still want to use legacy mode.So I want to know the address of CPU interface.

BR,

Peng

0 件の賞賛
返信