Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

1,574 次查看
charleshuang
Senior Contributor II

Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

If yes, can you tell me how to enable this function?

Thank you.

Best Regards,

Alex Cheng

标签 (5)
0 项奖励
回复
1 回复

907 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alex

chromium-imx recipes support hardware acceleration, refer to attached

Yocto Guide sect.5.6.6 Chromium Browser on X11, XWayland and Wayland

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复