How to change i.MX6SDL OCOTP write latencies.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to change i.MX6SDL OCOTP write latencies.

1,022 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a quesion about i.MX6SDL OCOTP.

Please see chapter 47.3.1.3 in IMX6SDLRM Rev.2, it says as following.

"It should be noted that write latencies to OTP are numbers of 10 micro-seconds per word.

Write latencies is based on amount of bit filed which is 1. For example : program half

fuse bits in one word need 10 us x 16."

Then, how can I change the write latencies?

By HW_OCOTP_TIMING[STROBE_PROG]?

Best Regards,

Satoshi Shimoda

标记 (1)
0 项奖励
回复
1 回复

907 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please follow recommendations of section 47.3.3 (OTP Read/Write Timing Parameters)

of the Reference Manual. Strictly speaking, it is not good idea to change significantly timings.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复