Does i.MX6 have internal EEPROM(or other internal volatile memory)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX6 have internal EEPROM(or other internal volatile memory)?

602件の閲覧回数
flagbee
Contributor I

I'd like to use an internal volatile memory such as EEPROM.

Does i.MX6 have internal EEPROM(or other internal volatile memory)?

ラベル(1)
0 件の賞賛
返信
1 返信

546件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Yes, the i.MX6 have the internal EEPROM, 512K, but it is only for uboot and it already be firmware. So you can not use it.
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信