Does i.MX6 have internal EEPROM(or other internal volatile memory)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 have internal EEPROM(or other internal volatile memory)?

603 Views
flagbee
Contributor I

I'd like to use an internal volatile memory such as EEPROM.

Does i.MX6 have internal EEPROM(or other internal volatile memory)?

Labels (1)
0 Kudos
Reply
1 Reply

547 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Yes, the i.MX6 have the internal EEPROM, 512K, but it is only for uboot and it already be firmware. So you can not use it.
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply