Hi
Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?
Yellow ---> MIPI_CSI_CLK
Green ---> MIPI_D0
Base on Debug steps for customer MIPI sensor.docx
3. Check every register of MIPI CSI-2 with MIPI_CSI_N_LANES ~ MIPI_CSI_DATA_IDS_2.
Tips:
I think 0x330 and 0x300 is base on continuous clock LPS mode. Right ?
If non-continuous clock LPS mode , the value is 0x300 , 0x630 , Right ?
Hi Appolo
I think you are right, non-continuous clock is supported and
clock lane supports stop state.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We had connect to ISP.
We had set color bar command to ISP , and it had output.
We had check some iMX6Q MIPI_CSI Registetr
It is "0" in MIPI_CSI_ERR1/2.
MIPI_CSI_PHY_STATE : 0x300 , 0x630
IPUx_INT_STAT_1 is 0x00800000. (It is not the same as OV5640 , 0x00001000)
We can't see color bar in i.MX6 Display. (Just only block color in Display)
(System just only one MIPI_CSI. No parallel camera)
(My test command is
./mxc_v4l2_overlay.out -di /dev/video0 -iw 1920 -ih 1080 -ow 1024 -oh 768 -fr 30 -m 5 -r 0 -fg
IPU1_CSI1_DI , IPU1_CSI1_SENS_CONF , IPU1_CSI1_SENS_FRM_SIZE , IPU1_CSI1_ACT_FRM_SIZE is the same as demo board.
Does any register need to check ?