Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?

1,935 Views
Danube
Contributor IV

Hi

Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?

Yellow ---> MIPI_CSI_CLK

Green ---> MIPI_D0

non_con.jpg

Base on Debug steps for customer MIPI sensor.docx

3. Check every register of MIPI CSI-2 with MIPI_CSI_N_LANES ~ MIPI_CSI_DATA_IDS_2.

Tips:

  • In ov5640_mipi case (2 data lanes are used), the correct MIPI_CSI_PHY_STATE is 0x330 (and the bit 11 is jumping between 0 and 1, the value is jump between 0x330 and 0x300.

I think 0x330 and 0x300 is base on continuous clock LPS mode. Right ?

If non-continuous clock LPS mode , the value is 0x300 , 0x630 , Right ?

Labels (6)
0 Kudos
4 Replies

914 Views
igorpadykov
NXP Employee
NXP Employee

Hi Appolo

I think you are right, non-continuous clock is supported and

clock lane supports stop state.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

914 Views
Danube
Contributor IV

Hi  igorpadykov

We can't see color bar in i.MX6 Display. (Just only block color in Display)

(System just only one MIPI_CSI. No parallel camera)

(My test command is

./mxc_v4l2_overlay.out -di /dev/video0 -iw 1920 -ih 1080 -ow 1024 -oh 768 -fr 30 -m 5 -r 0 -fg

IPU1_CSI1_DI , IPU1_CSI1_SENS_CONF , IPU1_CSI1_SENS_FRM_SIZE , IPU1_CSI1_ACT_FRM_SIZE is the same as demo board.

Does any register need to check ?

0 Kudos

914 Views
igorpadykov
NXP Employee
NXP Employee

Hi Appolo

sorry, I got updated info:

IC designer confirmed: The Non-continue clock transmission can’t be support by our DSI in i.mx6 series

~igor

0 Kudos

914 Views
igorpadykov
NXP Employee
NXP Employee

Hi Appolo

one can check

Debug steps for customer MIPI sensor.docx

~igor

0 Kudos