Do you know where I can become an Ecxel Sheet with the pinout information of the i.MX 6Solo/6DualLite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you know where I can become an Ecxel Sheet with the pinout information of the i.MX 6Solo/6DualLite

ソリューションへジャンプ
1,353件の閲覧回数
rainerscalick
Contributor I

I am searching for the pinout information about the i.MX6 solo and dual light (it think the are the same)

would be grat if you can help me.

ラベル(1)
タグ(2)
1 解決策
854件の閲覧回数
Yuri
NXP Employee
NXP Employee

It may be recommended to use the IOMUX tool, Excel tables for i.MX6 (as it took place
for previous devices of i.MX series) are not provided.

https://www.freescale.com/webapp/Download?colCode=IMX6_IOMUX_TOOL&appType=license&location=null&fasp...

i.MX6S|i.MX 6Solo Processors|Multimedia|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
854件の閲覧回数
art
NXP Employee
NXP Employee

There is no dedicated Excel sheet for the i.MX6Solo pinout. However, there is the IOMUX tool for the i.MX6 series processors, available for download on the Freescale web site (please check under the "Initialization/Boot/Device Driver Code Generation" tab):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6S&fpsp=1&tab=Design_Tools_Tab

that contains the detailed pinmux information for the i.MX6 series processors and simplifies the IOMUX configuration. In particular, it contains the detailed pinmux sheet (run the tool and check the "Pads" tab).

0 件の賞賛
返信
855件の閲覧回数
Yuri
NXP Employee
NXP Employee

It may be recommended to use the IOMUX tool, Excel tables for i.MX6 (as it took place
for previous devices of i.MX series) are not provided.

https://www.freescale.com/webapp/Download?colCode=IMX6_IOMUX_TOOL&appType=license&location=null&fasp...

i.MX6S|i.MX 6Solo Processors|Multimedia|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------