Do you know where I can become an Ecxel Sheet with the pinout information of the i.MX 6Solo/6DualLite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you know where I can become an Ecxel Sheet with the pinout information of the i.MX 6Solo/6DualLite

Jump to solution
1,239 Views
rainerscalick
Contributor I

I am searching for the pinout information about the i.MX6 solo and dual light (it think the are the same)

would be grat if you can help me.

Labels (1)
Tags (2)
1 Solution
740 Views
Yuri
NXP Employee
NXP Employee

It may be recommended to use the IOMUX tool, Excel tables for i.MX6 (as it took place
for previous devices of i.MX series) are not provided.

https://www.freescale.com/webapp/Download?colCode=IMX6_IOMUX_TOOL&appType=license&location=null&fasp...

i.MX6S|i.MX 6Solo Processors|Multimedia|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
740 Views
art
NXP Employee
NXP Employee

There is no dedicated Excel sheet for the i.MX6Solo pinout. However, there is the IOMUX tool for the i.MX6 series processors, available for download on the Freescale web site (please check under the "Initialization/Boot/Device Driver Code Generation" tab):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6S&fpsp=1&tab=Design_Tools_Tab

that contains the detailed pinmux information for the i.MX6 series processors and simplifies the IOMUX configuration. In particular, it contains the detailed pinmux sheet (run the tool and check the "Pads" tab).

0 Kudos
Reply
741 Views
Yuri
NXP Employee
NXP Employee

It may be recommended to use the IOMUX tool, Excel tables for i.MX6 (as it took place
for previous devices of i.MX series) are not provided.

https://www.freescale.com/webapp/Download?colCode=IMX6_IOMUX_TOOL&appType=license&location=null&fasp...

i.MX6S|i.MX 6Solo Processors|Multimedia|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------