Hi All,
I am working on imx7s board. I want to configure DMA to capture I2S data. I want to perform this activity from Cortex M4 core.
I have FreeRTOS package for this SoC. But currently DMA driver for FreeRTOS is not available can anyone please help for getting support for this?
Thanks,
Vivek
I don't know the ins and outs of what you are trying to do, or the drivers that are available, but if there is a 'bare metal' DMA driver available then you should be able to use that with FreeRTOS to. For example, if you want a task to respond to a DMA transfer then you could use the DMA interrupt along with a direct to task notification to unblock the task in a similar way as described on this page.
Thank you Richard for helping me understanding DMA integration design in FreeRTOS.
Hello Vivek
I'm looking also for a SDMA driver running of the M4 of the imx7d with RTOS. We would like to get capture data from the FTM (timer). Did you finally find existing software ?
Best regards
Jerome
I am not aware of rtos/'bare metal' i.MX7 sdma drivers, in general
one can try to design own scripts using
Thank you Igor..
This SDMA tutorial link is really helpful for understanding SDMA architecture and script writing for accessing it.
Also thanks for sharing link for Professional services.
Actually I need to capture I2S data (Using SAI interface) on SDMA and give interrupt to Cortex M4 core of Imx7s once enough data is available. I am not pretty sure whether I can do it using DMA scripts or not. Can you please let me know if that is possible? Also if possible, do NXP professional services provide support for this?
Thanks,
Vivek
Hi Vivek
this will require to create rtos sdma scripts, so may be
recommended to apply to NXP Professional Services:
http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------