Hello NXP Team,
I am trying to bring up a custom board which is using imx6 solo processor with different DDR3 SDRAM Configuration
I am trying to understand the following settings on SABRE solo board . Could you please explain
0x21b001c = 0x04008032
0x21b001c = 0x8033
0x21b001c = 0x48031:
Thanks,
Says
Solved! Go to Solution.
Thanks Igor !! One final question before I close this topic.
- From BSP porting document for configuring DDR3 I see free-scale mentioned about changing the *.cfg file in boards/mx6solosabresd/*.cfg file but I also see Plugin.s file in the same folder that has the same DCD table as the cfg file and from make file I see we are using plugin.s object file.
For board mx6solosabresd:
Could you please clarify if we should change the DCD table in *.cfg or plugin.s it looks like plugin.s is the assembly version of the *.cfg file.
Thanks,
Swapna
Hi Swapna
both options are equal, one can use them
on own choice.
Best regards
igor
Thank you Igor.
I already saw the reference manual but I am a bit confused with mode register setting.
For Ex: 0x21b001c = 0x04008032
The mode register address is 0x0400 and I couldn't figure this address from the DRAM manufacturer data sheet.
Could you please help?
Thanks. This was helpful.
- Can we use JTAG to initialize memory? Are there any scripts for JTAG and recommendations from freescale to bring up a custom board based on solo.?
I am looking at the uboot code board configuration files and they are *.cfg files with Device configuration Tables is this the only place to change the needed for custom board.
Appreciate your time!!
Hi Says
these records performs programming DDR chips Mode registers,
description can be found in sect.45.12.8 MMDC Core Special Command
Register (MMDCx_MDSCR) i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
and datasheets of used DDR parts.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------