Hi All,
I have a new iMX6ULL board with a 512MBx16 DDR RAM chip (ISSI IS43TR16512B-125KBL). I am trying to use the RAM Stress Test tool over JTAG. I have built an init script, based on the EVK example (which has a 512MB DDR instead of 1GB on our board), but have increased the number of rows from 15 to 16. I have been able to load the RAM test script via JTAG (my USB is not yet working). If I run with a RAM density of 512MB or less, it passes fine. However, if I change the density to 1GB, it fails with the following message:
DDR Freq: 396 MHz
t0.1: data is addr test
Address of failure(step2): 0xa0000000
Data was: 0x9fffffe0
But pattern should match address
Error: failed to run stress test!!!
If I turn off bank interleaving, it fails at this address:
DDR Freq: 396 MHz
t0.1: data is addr test
Address of failure(step2): 0x800000c0
Data was: 0x800000a0
But pattern should match address
Error: failed to run stress test!!!
So it appears to me that this is corresponding with the high bit of the row.
Does anyone have any ideas where I might be going wrong here?
The RAM is setup in MMDC_MDCTL as follows:
w4 0x021B0000, 0x85180000 // [MMDC_MDCTL] MMDC Core Control Register
// <31> SDE_0 , 1'b1: MMDC Enable CS0;
// <30> SDE_1 , 1'b0: MMDC Enable CS1;
// <26:24> ROW , 3'b101: set ROW Address Width, 3'b101 stands for 16bits Row;
// <22:20> COL , 3'b001: set COL Address Width, 3'b001 stands for 10bits Column;
// <19> BL , 1'b1: set Burst Length as 8;
// <17:16> DSIZ , 2'b00: set DDR Data Bus Size as 16-bit;
Is there anything else I need to setup?
已解决! 转到解答。