Current consumption by NVCC_xxx lines if not used (iMX6 Dual core).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current consumption by NVCC_xxx lines if not used (iMX6 Dual core).

462 Views
abhijit_mote
Contributor I

What would be the current requirements by all the peripheral supplies (NVCC_xxx) in case if they are not being used?

0 Kudos
Reply
1 Reply

392 Views
art
NXP Employee
NXP Employee

The current consumption on the I/O supply voltage rails NVCC_xxx depends on the IOMUX pad configuration (e.g. pad function selection, pull-up/down resistors enabling/disabling etc.) even when the corresponding pads are not switching. So, the actual IOUMUX configuration of the corresponding pads should be taken into the account to estimate the currnt consumption on the I/O supply voltage rails.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply