What would be the current requirements by all the peripheral supplies (NVCC_xxx) in case if they are not being used?
The current consumption on the I/O supply voltage rails NVCC_xxx depends on the IOMUX pad configuration (e.g. pad function selection, pull-up/down resistors enabling/disabling etc.) even when the corresponding pads are not switching. So, the actual IOUMUX configuration of the corresponding pads should be taken into the account to estimate the currnt consumption on the I/O supply voltage rails.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------