who have the patch about pcie bus on the linux 3.0.35?
I work on the imx6q ,when i debug pcie bus on the linux 3.0.35,there is some problem,however on the linux3.10.17,it's ok,so i want to have the patch about pcie on the linux3.0.35,or tell me the difference between linux 3.0.35 and linux3.10.17 about pcie bus;thanks
There is no separate patch for that since some problems of the 3.0.35 BSP (not only related with PCIe) were on the kernel level and newer kernel should be used to fix them.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------