Hello,
I was referring to EVK of i.MX6UL. However I could not not get the part numbers of crystal and Oscillator used on EVK.
Can anyone share me the part numbers of both.
Thanks,
Surendra
Hello,
Please use BOM file in design files package :
http://www.nxp.com/assets/downloads/data/en/schematics/MCIMX6UL-EVK_DESIGNFILES.zip
Summary page :
i.MX6UltraLite Evaluation Kit|NXP
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
After going through EVK of NXP I founf two resistors are added at the output of Oscillator.
I think they may be used to downconvert the 3.3V output to 1.1V(NVCC_PLL).
Same is shown with red circles in the attached image.
Let me know your inputs on this.
Regards,
Surendra.
Hello,
The i.MX6 UL TO 1.0 (Maskset ID:0N52P) has some issues. Please use the TO 1.1 (Maskset ID: 1N52P).
For this release the recent Hardware Development Guide for the i.MX 6UltraLite should be used.
http://www.nxp.com/assets/documents/data/en/user-guides/IMX6ULHDG.pdf
Please refer to 2.6 (Migrating from i.MX 6UltraLite TO1.0 to TO1.1).
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!