Consulting help: IMX.6q EIM sdma with upstream linux kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Consulting help: IMX.6q EIM sdma with upstream linux kernel

1,221件の閲覧回数
joshuaclayton
Contributor III

I have a hardware platform based on The IMX6.q , which does data acquisition.

Our in house driver does data collection through an fpga connected to the EIM bus.

I need to adapt the EIM driver to use SDMA with the upstream kernel.

Looking for consulting help with a dma engine and sdma script to replace the existing data interrupt.

Ideally doing it in a way that might at some future time be suitable for upstream.

Please contact me if you have the necessary combination of experience, and availability.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

625件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joshua

I would suggest to look at below links, suitable for fpga connected to the EIM bus

SDMA ap_to_ap Fixed Scripts (i.MX6DQ)

Freescale i.MX SDMA tutorial (part I)

https://github.com/rabeeh/android-imx6-kitkat/blob/master/platform/external/linux-test.git/0370-ENGR...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信