Hi,
I have bought a 10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1) which stated the display is dedicated for i.MX53.
Regarding the processor, I had bought a development board from Digi (Part No : CC-WMX53-LX) that has featured an i.MX53 processor and the LVDS port connector is DF14-30P-1.25H(25).
I was trying to connect the i.MX53 development board to the display through the LVDS port where both the connectors are not compatible.
I would like to ask if anyone knows the model number of the LVDS connector at the display panel so I could be able to make an adapter accordingly.
Many thanks.
Kind Regards,
Siu Ho
Hi,
Thanks for the reply.
I did a search from those components distributor website like RS and Farnell but they only have DF19G-30P-1H(54) rather than DF19G-30P-1H(56). Thus I would like to ask what's the difference between them and can I use DF19G-30P-1H(54) instead please?
And I would also like to confirm if the model number of the female port is DF19G-30S-1C(05)?
Many thanks.
Kind Regards,
Siu Ho