Connectivity of 10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1)

cancel
Showing results for 
Search instead for 
Did you mean: 

Connectivity of 10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1)

331 Views
siuho
Contributor I

Hi,

I have bought a 10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1) which stated the display is dedicated for i.MX53.

Regarding the processor, I had bought a development board from Digi (Part No : CC-WMX53-LX) that has featured an i.MX53 processor and the LVDS port connector is DF14-30P-1.25H(25).

I was trying to connect the i.MX53 development board to the display through the LVDS port where both the connectors are not compatible.

I would like to ask if anyone knows the model number of the LVDS connector at the display panel so I could be able to make an adapter accordingly.

Many thanks.

Kind Regards,

Siu Ho

Labels (1)
0 Kudos
2 Replies

84 Views
4guin4g4
Contributor IV

Acording to the information on the design files

it is a DF19G-30P-1H(56), Manufacturer: HIROSE

84 Views
siuho
Contributor I

Hi,

Thanks for the reply.

I did a search from those components distributor website like RS and Farnell but they only have DF19G-30P-1H(54) rather than DF19G-30P-1H(56). Thus I would like to ask what's the difference between them and can I use DF19G-30P-1H(54) instead please?

And I would also like to confirm if the model number of the female port is DF19G-30S-1C(05)?

Many thanks.

Kind Regards,

Siu Ho

0 Kudos