Hi
I am looking to monitor my external Clipped Sine Wave TCXO 40MHZ using iMX6DL (Signal "EPIT1_OUT").
I have attached my use case and also one content 31.2.1 from iMX6DL saying input clock should be 1/4 frequency of the Peripheral Clock.
Can i use Timer/Capture pin to monitor my TCXO external Clock?
imx6-x
Regards
Nitesh
Hi Igor
Thanks for the reply.
Is there any way i can monitor 40MHz TCXO Clipped Sine wave using iMX6DL.
Regards
Nitesh
Hi Nitesh
I think this is not possible.
Best regards
igor
Hi Nitesh
"Peripheral Clock" or peripheral clock (ipg_clk) as described in Reference Manual
is IPG_CLK_ROOT value and provided in Table 18-4. System Clock Frequency Values i.MX6SDL
Reference Manual. Seems 40MHZ can not be used.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------