Hello,
We're using i.MX6Q Linux 3.10.17_1.0.0_ga on SabreSD board, configured as PCIe RC.
Attached propiatery EP device on PCIe has three 32-bit BARs, 1MBytes each. Registers of interest on EP go from address 0x01000000 on.
On i.MX6 Linux performs the following BAR mapping:
32-bit BAR0 - 1MByte: 0x01200000 - 0x12FFFFF
32-bit BAR1 - 1MByte: 0x01300000 - 0x13FFFFF
32-bit BAR2 - 1MByte: 0x01300000 - 0x13FFFFF
Without using iATU we can only access registers on EP from address 0x01200000 on.
We've tried enabling iATU in file drivers/pci/host/pci-imx6.c as described below, but the address translation didn't work (we've got the same register content as prior enabling iATU)
writel(0, pp->dbi_base + PCIE_ATU_VIEWPORT);
writel(0x01000000, pp->dbi_base + PCIE_ATU_LOWER_BASE);
writel(0x00000000, pp->dbi_base + PCIE_ATU_UPPER_BASE);
writel(0x010fffff, pp->dbi_base + PCIE_ATU_LIMIT);
writel(0x00200000, pp->dbi_base + PCIE_ATU_LOWER_TARGET);
writel(0x00000000, pp->dbi_base + PCIE_ATU_UPPER_TARGET);
writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);
writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);
I would appreciate any suggestions or ideas how to make iATU operational to access registers on EP from 0x01000000 on.
Best regards,
解決済! 解決策の投稿を見る。
Solution is described below (base/target addresses were incorrect - reference manual a bit misleading)
#define BAR0_ADDR 0x01200000
#define VTSS_ADDR 0x01000000
writel(2, pp->dbi_base + PCIE_ATU_VIEWPORT); // 0 and 1 are already used in pcie-designware.c
writel(BAR0_ADDR, pp->dbi_base + PCIE_ATU_LOWER_BASE);
writel(0, pp->dbi_base + PCIE_ATU_UPPER_BASE);
writel(BAR0_ADDR + SZ_1M - 1, pp->dbi_base + PCIE_ATU_LIMIT);
writel(VTSS_ADDR, pp->dbi_base + PCIE_ATU_LOWER_TARGET);
writel(0, pp->dbi_base + PCIE_ATU_UPPER_TARGET);
writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);
writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);
Solution is described below (base/target addresses were incorrect - reference manual a bit misleading)
#define BAR0_ADDR 0x01200000
#define VTSS_ADDR 0x01000000
writel(2, pp->dbi_base + PCIE_ATU_VIEWPORT); // 0 and 1 are already used in pcie-designware.c
writel(BAR0_ADDR, pp->dbi_base + PCIE_ATU_LOWER_BASE);
writel(0, pp->dbi_base + PCIE_ATU_UPPER_BASE);
writel(BAR0_ADDR + SZ_1M - 1, pp->dbi_base + PCIE_ATU_LIMIT);
writel(VTSS_ADDR, pp->dbi_base + PCIE_ATU_LOWER_TARGET);
writel(0, pp->dbi_base + PCIE_ATU_UPPER_TARGET);
writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);
writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);