Configuring iATU on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring iATU on i.MX6

ソリューションへジャンプ
2,916件の閲覧回数
gasperkorinsek
Contributor I

Hello,


We're using i.MX6Q Linux 3.10.17_1.0.0_ga on SabreSD board, configured as PCIe RC.


Attached propiatery EP device on PCIe has three 32-bit BARs, 1MBytes each. Registers of interest on EP go from address 0x01000000 on.


On i.MX6 Linux performs the following BAR mapping:

32-bit BAR0 - 1MByte: 0x01200000 - 0x12FFFFF

32-bit BAR1 - 1MByte: 0x01300000 - 0x13FFFFF

32-bit BAR2 - 1MByte: 0x01300000 - 0x13FFFFF

Without using iATU we can only access registers on EP from address 0x01200000 on.


We've tried enabling iATU in file drivers/pci/host/pci-imx6.c as described below, but the address translation didn't work (we've got the same register content as prior enabling iATU)


writel(0, pp->dbi_base + PCIE_ATU_VIEWPORT);

writel(0x01000000, pp->dbi_base + PCIE_ATU_LOWER_BASE);

writel(0x00000000, pp->dbi_base + PCIE_ATU_UPPER_BASE);

writel(0x010fffff, pp->dbi_base + PCIE_ATU_LIMIT);

writel(0x00200000, pp->dbi_base + PCIE_ATU_LOWER_TARGET);

writel(0x00000000, pp->dbi_base + PCIE_ATU_UPPER_TARGET);

writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);

writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);

I would appreciate any suggestions or ideas how to make iATU operational to access registers on EP from 0x01000000 on.

Best regards,

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,325件の閲覧回数
gasperkorinsek
Contributor I

Solution is described below (base/target addresses were incorrect - reference manual a bit misleading)

#define BAR0_ADDR 0x01200000

#define VTSS_ADDR 0x01000000


writel(2, pp->dbi_base + PCIE_ATU_VIEWPORT); // 0 and 1 are already used in pcie-designware.c

writel(BAR0_ADDR, pp->dbi_base + PCIE_ATU_LOWER_BASE);

writel(0, pp->dbi_base + PCIE_ATU_UPPER_BASE);

writel(BAR0_ADDR + SZ_1M - 1, pp->dbi_base + PCIE_ATU_LIMIT);


writel(VTSS_ADDR, pp->dbi_base + PCIE_ATU_LOWER_TARGET);

writel(0, pp->dbi_base + PCIE_ATU_UPPER_TARGET);

writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);

writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,326件の閲覧回数
gasperkorinsek
Contributor I

Solution is described below (base/target addresses were incorrect - reference manual a bit misleading)

#define BAR0_ADDR 0x01200000

#define VTSS_ADDR 0x01000000


writel(2, pp->dbi_base + PCIE_ATU_VIEWPORT); // 0 and 1 are already used in pcie-designware.c

writel(BAR0_ADDR, pp->dbi_base + PCIE_ATU_LOWER_BASE);

writel(0, pp->dbi_base + PCIE_ATU_UPPER_BASE);

writel(BAR0_ADDR + SZ_1M - 1, pp->dbi_base + PCIE_ATU_LIMIT);


writel(VTSS_ADDR, pp->dbi_base + PCIE_ATU_LOWER_TARGET);

writel(0, pp->dbi_base + PCIE_ATU_UPPER_TARGET);

writel(PCIE_ATU_TYPE_MEM, pp->dbi_base + PCIE_ATU_CR1);

writel(PCIE_ATU_ENABLE, pp->dbi_base + PCIE_ATU_CR2);

0 件の賞賛
返信